Part Number: TMS320F28377D
Dear experts,
As I understand it, if SCCRESET is triggered on CPU1, CPU2 will also be reset.
If I trigger SCCRESET from CPU1, what is the boot flow of CPU2 after its reset?
Since the user manual describes the CPU2 boot ROM action as "No Action," what will the boot flow be after the reset? Will CPU2 start from the start address (for example, 0x80000) and then jump to the entry point symbol (c_int00)?
Thanks and Regards,
C.C.Liu