Part Number: TMS320F28335
Hi,
I am facing issue related to "/28335_RAM_lnk.cmd", line 132 error#10099-D program will not fit into available memory. Kindly help me.
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x000000, length = 0x000002 /* Boot to M0 will go here */
RAMM0 : origin = 0x000050, length = 0x0003B0
RAML0 : origin = 0x008000, length = 0x001000
RAML1L2L3 : origin = 0x009000, length = 0x003000
// RAML1 : origin = 0x009000, length = 0x001000
// RAML2L3 : origin = 0x00A000, length = 0x002000
// RAML2 : origin = 0x00A000, length = 0x001000
// RAML3 : origin = 0x00B000, length = 0x001000
ZONE7A : origin = 0x200000, length = 0x00FC00 /* XINTF zone 7 - program space */
CSM_RSVD : origin = 0x33FF80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
CSM_PWL : origin = 0x33FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
ADC_CAL : origin = 0x380080, length = 0x000009
RESET : origin = 0x3FFFC0, length = 0x000002
IQTABLES : origin = 0x3FE000, length = 0x000b50
IQTABLES2 : origin = 0x3FEB50, length = 0x00008c
FPUTABLES : origin = 0x3FEBDC, length = 0x0006A0
BOOTROM : origin = 0x3FF27C, length = 0x000D44
PAGE 1 :
/* BOOT_RSVD is used by the boot ROM for stack. */
/* This section is only reserved to keep the BOOT ROM from */
/* corrupting this area during the debug process */
BOOT_RSVD : origin = 0x000002, length = 0x00004E /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAML4 : origin = 0x00C000, length = 0x001000
RAML5 : origin = 0x00D000, length = 0x001000
RAML6 : origin = 0x00E000, length = 0x001000
RAML7 : origin = 0x00F000, length = 0x001000
ZONE7B : origin = 0x20FC00, length = 0x000400 /* XINTF zone 7 - data space */
}
SECTIONS
{
/* Setup for "boot to SARAM" mode:
The codestart section (found in DSP28_CodeStartBranch.asm)
re-directs execution to the start of user code. */
codestart : > BEGIN, PAGE = 0
ramfuncs : > RAML0, PAGE = 0
.text >> RAML1L2L3|RAMM0|RAML0, PAGE = 0
//.text >> RAML1|RAML2|RAMM0|RAML0|RAML3, PAGE = 0
// .text : > RAML1, PAGE = 0
.cinit : > RAML0, PAGE = 0
.pinit : > RAML0, PAGE = 0
.switch : > RAML0, PAGE = 0
.stack : > RAMM1, PAGE = 1
.ebss : > RAML4, PAGE = 1
.econst : > RAML5, PAGE = 1
.esysmem : > RAMM1, PAGE = 1
IQmath >> RAML1L2L3, PAGE = 0
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
/*
codestart : > BEGIN, PAGE = 0
ramfuncs : > RAML0, PAGE = 0
.text >> RAML1|RAML2L3|RAMM0|RAML0, PAGE = 0
//.text >> RAML1|RAML2|RAMM0|RAML0|RAML3, PAGE = 0
// .text : > RAML1, PAGE = 0
.cinit : > RAML0, PAGE = 0
.pinit : > RAML0, PAGE = 0
.switch : > RAML0, PAGE = 0
.stack : > RAMM1, PAGE = 1
.ebss : > RAML4, PAGE = 1
.econst : > RAML5, PAGE = 1
.esysmem : > RAMM1, PAGE = 1
IQmath : > RAML1, PAGE = 0
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
DMARAML4 : > RAML4, PAGE = 1
DMARAML5 : > RAML5, PAGE = 1
DMARAML6 : > RAML6, PAGE = 1
DMARAML7 : > RAML7, PAGE = 1
ZONE7DATA : > ZONE7B, PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used */
csm_rsvd : > CSM_RSVD PAGE = 0, TYPE = DSECT /* not used for SARAM examples */
csmpasswds : > CSM_PWL PAGE = 0, TYPE = DSECT /* not used for SARAM examples */
/* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
.adc_cal : load = ADC_CAL, PAGE = 0, TYPE = NOLOAD
}