Part Number: TMS320F28051
Hello,
In terms of Flash sizes, when looking at the description of the TMS320F28051 on its product page, I see the following - "C2000 32-bit MCU with 60 MHz, 64 KB flash, PGAs, 2 MSPS ADC".
But, when looking at the comparison table in datasheet I see the following (highlighted in yellow):

Can you confirm that these two are equal (32K * 16 bits = 32K * 2 bytes = 64KB)? If so, can you help me understand why these numbers are provided in two different formats in these different places?
Thanks!