Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hello,
I am trying to use the PWM deadband configuration for one of my application. I have PWM low signal that has been derived from the PWM high signal and it is coplementary. I have the below picture that explains the deadband module configuration in my application. Highlighted switches and the configurations has been ebabled.

I have the PWM clock (TBCLK) configured for 200MHz and DBRED and DBFED programed for 100 to get the dead band time of 500 nano sec. I expect to see Raising edge will have 500nsec deadtime and Falling edge also will have 500nsec deadtime. However, i witnessed, raising edge is having 400nsec dead time and falling edge is having 600nsec deadtime.
Repeated the same excersite with 300nano sec dead time on both raising and falling edge. Witnessed that, Raising Edge is having 200nsec deadtime and falling edge havinf 400nsec deadtime.
Why the PWM deadtime is not equal on both the edges (Falling and Raising)?
Please help.
Thanks,
Munaf