Part Number: TMS320F280039C
Based on the TRM.Table5-1 description, if both Zone1 and Zone2's GRABRAMx/GRABSECTx Bits is config to 11, then RAM block/Flash Sector inaccessible if either of the zone is secure (CSM passwords are programmed). Never leave these values as default (11), if CSM passwords are programmed for even one zone.
My question :
1. What meaning of "either of the zone is secure (CSM passwords are programmed)" ? If I config both Zone1 and Zone2's GRABRAMx/GRABSECTx Bits is config to 11, and I programmed CSM passwords, then the RAM/FLASH cannot be access even if I am not lock any Zone(config DCSM_Zx_REGS.Zx_CR.FORCESEC)?
2. In the TRM of TMS280025C Table 3-16, when both Zone1 and Zone2's GRABRAMx/GRABSECTx Bits is config to 11, the description is “RAM block/Flash Sector is unsecure when both
of the zones are UNLOCKED, otherwise memory region is inaccessible if either of the two zones are LOCKED”. The protection logic for 280025 and 280039 in this part are same?