Part Number: TMS320F28379S
Hi, I have a design using the TMS320F28379SZWTT device and the s/w is done in Matlab/Simulink.
Hopefully a simple question! I have one o/p GPIO16 that is outputting a 500Hz square wave, but in my model I have GPIO16 connected to a constant block, which I can change between 0 & 1 but this makes no difference and it always o/ps the square wave. The h/w settings for the GPIO port look correct and are the same as all the other GPIO o/ps that are working correctly.
Is there a way to see if anything else is using this GPIO?
Thanks
Ian