Other Parts Discussed in Thread: UNIFLASH,
Tool/software:
We are using TMS320F28P650DH. Currently use CPU1 and CLA, it works well. But use uniflash program tool to program CPU2 project, it can't be program.
We are not sure if it is CPU2 project issue or uniflash setting issue.
we got the demo from c2000 ware (dual CPU). but the CPU2 is empty project. We add code in the project. Not sure if it is correct.
Hope that you can kindly share the demo code that include CPU1/CLA/CPU2. The simple code can control GPIOs status. For example: CPU1 control the GPIO0, CPU2 control GPIO1, CLA control GPIO2.
Thank you very much.