Part Number: TMS320F2800157
Other Parts Discussed in Thread: LAUNCHXL-F2800157, C2000WARE
Tool/software:

The problem is described as follows:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F2800157
Other Parts Discussed in Thread: LAUNCHXL-F2800157, C2000WARE
Tool/software:

The problem is described as follows:
Hi Jianping,
The .out file will be present inside the CPU1_RAM folder.
Thanks
Aswin
At present, it is impossible to generate a .out file, please help solve this problem, thank you!
Hi,
If you need to build and run the example in Launchpad, please update the build settings.
Right click on the project -> build configuration -> set active -> cpu1_launchxl_ram

You dont need to change any other properties from the project for building it.
For building the example, right click on the project -> click on the rebuild option
You should be able to find the .out file inside the CPU1_LaunchXL_RAM folder

Let me know if this resolved your issue, else please zip the project and attach to the post, i will analyse further.
Thanks
Aswin
Hi,
Were you able to get the .out file after building?
Please close this thread if you are able to resolve the .out issue and create a new thread with the issue that you are facing related to interrupt.
Thanks
Aswin
1. The customer's previous project can generate .out files, but the official routine still can't generate .out files, and the reason has not been found yet;(1. The customer uses CCS12.7.1 (10 May 2024)+C2000ware, and the hardware platform is in the LAUNCHXL-F2800157 evaluation board that we officially applied)
2. Help to see the problem of interrupting, see the attachment for the specific code, thank you!


Hi,
Did you follow the same steps as mentioned above for building the example?
Please use latest CCS V12.7 and latest C2000Ware SDK V 5.02 . Let me loop CCS experts to address this issue.
Help to see the problem of interrupting, see the attachment for the specific code, thank you!
Please create a separate thread to address this issue, so that we can assign to the respective subject matter experts.
Thanks
Aswin