Tool/software:
Hello,
As showd in the picture, it tries to push the AL onto stack.
But after the execution of this command, the content in the stack is not the AL.
The cpu has write access to the memory. The memory is in TEST mode with Only write to data bits, not ECC bits.
what can be the reason? I can set the value at that address via debugger to e.g. 8a20, 8a00, 8a17, but i cant set it to 8a18.
Thanks.