Part Number: TMS320F280049C
Other Parts Discussed in Thread: LAUNCHXL-F280049C, C2000WARE, TIDM-02011
Tool/software:
Hi,
I wanted to perform Live firmware upgrade and referring SPRUIU8a, following the steps as mentioned in 6.2.
Hardware Used: LAUNCHXL-F280049C
Development Environment: CCS Theia
Using "flashapi_ex2_sci_kernel" as SCI bootloader and "flashapi_ex3_live_firmware_update" application firmware
Problem Statement:
In the first step when i am loading SCI kernel in BANK0 via CCS and loading "flashapi_ex3_live_firmware_updateBANK1FLASH.txt" in BANK1 via cmd. After doing reset, board is working same as explained in document means blink of LED2. But, when i am loading SCI Kernel in BANK1 via CCS and loading "flashapi_ex3_live_firmware_updateBANK0FLASH.txt" in BANK0 via cmd. Then after doing reset, board is not working means LED1 is not blinking. I don't know memory is corrupting or what can be the issue.
One point i observed, if i am loading kernel in any BANK then i can download the application image only once. For downloading application image again then i need to load the SCI kernel again. Is it a desired behavior?
Regards