Part Number: TMDSCNCD28P65X
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello there,
Got the SPI Module running at desired SPYCLK rate etc.
Trying to maximize the speed of SPYCLK up to 50 MHz of advertised limitation. Seems to be able to.
The problem is setting the "Enable High Speed Mode" in the syscfg file. It changes the PinMux settings and allow only certain GPIOs to be selected.
In particular GPIO58, GPIO59, and GPIO60, for SPI_PICO, SPI_POCI, and SPI_CLK.
The EVM Pinout map shows GPIO60 at pin # 125, and it has the clock signal out. Problem is finding GPIO58 and GPIO59, where do this signals go? Is there an updated pin out document?
Is there other High Speed capable pins? How to set the PinMux to access them?
Please help out with these SPI High speed mode questions.
Regards,
Sergey.