This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
We have been using TI TMS320F28388D MCU in one of our product requiring UL1998 / IEC60730-1 safety standard compliance.
Could you please confirm if IEC60730 safety library is available for TMS320F28388? If yes, please share same with us.
If not then please help/guide on developing the diagnostic safety library for MCU TMS320F28388D.
Thanks and Regards,
Dnyaneshwar Kashid
Hi Dnyaneshwar,
We no longer provide a full IEC60730 library like F2837x device, since we later realized that many of the functions provided in the library are very application specific, and cannot be reused by customers as-is anyways.
We do provided a software diagnostic library for the F2838x device in C2000ware release, which includes many tests in the IEC60730, such as a CPU register test. You can find the library from the below folder within C2000ware installation. Thanks.
C2000Ware_xxxxxxxx\libraries\diagnostic\f2838x
Han