Part Number: TMS320F28379D
Tool/software:
Hi everyone,
I am working on a radiation detection project. I need to sample the output of amplifier circuit (Cremat) with ADC in C2000 Launchpad. I am sure that the code and connections are ok. When I measure the output of the amplfier by oscilloscope, I can see the gamma peak which is shown in picture below. However, when I conenct the output of the amplifier to the ADC input of C2000, I see strange data on the graph. could you please help me if I miss somethnig like impedance matching etc.?