This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
1. Is it correct that the output is 0V when PWM duty cycle is 50%?
2. If the answer to question 1 is yes, does the voltage vary between 50% and 100% duty cycle?
3. Based on the "tiduai7" document, the results were as follows:
- At 50% PWM, a boost from 12V to 400V occurred (the document states 0V at 50%).
- FET damage occurred when controlling from 0% duty cycle.
I am unsure if these results are due to my misunderstanding of the circuit and code. Could you provide a brief explanation of how the boost operation works?