Part Number: TMS320F28388D
Tool/software:
Hi ,
Referring to a previous post: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1358929/tms320f28388d-bga-package-layout-guidance
The datasheet states "There is a 50-kΩ internal pulldown on this pin in both an ADC input or DAC output mode which cannot be disabled." but doesn't give an indication of the tolerance of this pulldown.
Customer had a separate question regarding internal pull-downs on the analog inputs ADCINA0, ADCINA1, and ADCINB1. The datasheet states that they are a 50kOhm nominal value, but doesn't give a range.
What's the expected tolerance of this internal pulldown?
The datasheet states "There is a 50-kΩ internal pulldown on this pin in both an ADC input or DAC output mode which cannot be disabled." but doesn't give an indication of the tolerance of this pulldown.
Thanks, and regards,
Obinna.