This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I noticed that InstaSPIN-FOC supports chips such as F28027F, I am now wondering if it is possible to use this library on F280025? For example, I don't use FAST
Hello,
Thanks for your inquiry. This expert is currently out of office. Please expect 1-2 days delay in response - thanks for your patience!
Best Regards,
Allison
Yes. We have provided a software FAST library based solution that can support InstaSPIN with FAST on all of the C2000 devices with FPU. You may refer to the lab for the newer C2000 device in motor control SDK. The universal motor control lab is available in the current MCSDK, which can support a set of hardware kits and control algorithms for BLDC/PMSM drive. The kits include LAUNCHXL-F280025C, LAUNCHXL-F280039C, LAUNCHXL-F2800137 with BOOSTXL-DRV8323RS, BOOSTXL-DRV8323RH, DRV8353Rx-EVM, BOOSTXL-3PHGANINV, DRV8316REVM, or DRV8329AEVM inverter board for low voltage motor (max: 100Vdc) . TMDSCNCD280025C, TMDSCNCD2800137 , TMDSCNCD2800157 , or TMDSCNCD280039C with TMDSHVMTRINSPIN inverter board and TMDSADAP180TO100 for high voltage motor (max 350Vdc). And The control algorithms include sensorless InstaSPIN-FOC with FAST, Sensorless-FOC with eSMO, Sensored-FOC with incremental encoder, Sensored-FOC with hall sensor.
C2000WARE-MOTORCONTROL-SDK: https://www.ti.com/tool/C2000WARE-MOTORCONTROL-SDK
Universal Project and Lab User’s Guide: https://www.ti.com/lit/spruj26
Example lab project at the folder: C:\ti\c2000\C2000Ware_MotorControl_SDK_<version>\solutions\universal_motorcontrol_lab\f28002x
or C:\ti\c2000\C2000Ware_MotorControl_SDK_<version>\solutions\universal_motorcontrol_lab\f28003x
or C:\ti\c2000\C2000Ware_MotorControl_SDK_<version>\solutions\universal_motorcontrol_lab\f280013x
or C:\ti\c2000\C2000Ware_MotorControl_SDK_<version>\solutions\universal_motorcontrol_lab\f280015x
I noticed that there is a FAST submenu under the MotorWare directory, but there are only 2802x, 2805x, 2806x in FAST,
It's under Motor Control SDK as mentioned above, not motorWare.
can I use FAST on a chip with FPU like 280025?
Yes.
If not, can eSMO be used to estimate rotor position?
Yes.