This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28379D: powered the daughterboard without the docking station

Part Number: TMDSCNCD28379D
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hello, I would like to power the TMDSCNCD28379D daughterboard directly without powering or using the THDSHSECDOCK. I ordered connectors compatible with the TMDSCNCD28379D, but I do not know and I do not find which of the 180 pin should I power my + 5 V. Is the power supply connected to the A:J1 connection (mini usb) or to one of the 180 pins on the card connector?
Thank you in advance for your reply.

Florentin