This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: CAN data reception

Part Number: TMS320F28335

Tool/software:

F28335 CAN data reception, when CAN register CRCE set up, this frame of data will also be stored in the receiving mailbox?

  • There is not a register called CRCE. If a coming CAN message passes the acceptance filter, the message will be stored into a mailbox. The CAN messages are filtered using an Identifier or a range of identifiers. The mailbox should be configured for receiving message. 

    The CAN bus is a simple architecture where multiple nodes are connected on the same two wired structures (CAN_H and CAN_L). The transmitted data follows the arbitration process, and the signal transmitted is received by every single node. It is on the nodes to decide if they wish to accept or reject any data that is being transmitted to them on the CAN bus.