Tool/software:
Newer got an answer on this (original thread is locked)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As per engineering, the warning can be safely ignored and should be suppressed. It should be OK to reference additional projects in the system.
Regarding:
In case the warning is to be ignored:
In the meantime i look forward to the reply from the experts. :-)
For a workaround, can you try manually adding a line like the one below into the <system> element in the system.xml file:
<system> . . . <project configuration="@match" id="project_<some-random-number>" name="BOOTLOADER"/> </system>
For a permanent solution, we will file a bug for this to address in a future CCS version.