Other Parts Discussed in Thread: C2000WARE
Tool/software:
How can I use the C2000-SAFETI-DIAGNOSTICS-LIB in an EABI project when existing .lib files are COFF ABI?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
How can I use the C2000-SAFETI-DIAGNOSTICS-LIB in an EABI project when existing .lib files are COFF ABI?
For now there is no If you wish to use the C2000-SAFETI-DIAGNOSTICS-LIB in an EABI project, for now you will need to take a few steps to migrate the library to EABI yourself as there is currently no officially released EABI version
First, note that the C2000-SAFETI-DIAGNOSTICS-LIB is for F2807x and F2837x devices only. Support for F2800x, F2838x, and F28Px devices are already available for EABI in C2000Ware under the libraries/diagnostic/.
It will also help to acquaint yourself with COFF to EABI migration in general. Please see the C2000 Migration from COFF to EABI page for details. These steps also assume you have some familiarity with C2000Ware and the structure of the SDL.
STEP 1. At the root of the SDL directory, there is a CCS folder (e.g. \libraries\diagnostic\f2837xd\ccs) that contains a .projectspec for a static library project that can be used to rebuild the SDL .lib files. Start by importing this project into CCS and updating the project properties to set the output format to EABI.
Note that the project has 4 different build configurations that will all need to be updated to EABI. Alternatively you can add new build configs for EABI if you want to retain the ability to build COFF libraries, although you'll want to update the archiver settings to give the output file a unique name (e.g. F2837xD_Diagnostic_STL_CPU1_DEBUG_EABI.lib)
STEP 2. The SDL has a dependency on the Driverlib and the SFO (HRPWM calibration) libraries. You will similarly need EABI versions of these libraries. The easiest way to do this is to get them from a newer version of C2000Ware where they have already been migrated. Versions newer than C2000Ware 3.00.00 should have support for this.
STEP 3. The majority of the changes you will need to make to port the library are related to assembly code. The migration guide mentioned above describes these update in the Assembly Code Changes section. In the .asm files in the library source folder, you will need to remove the COFF underscores from the function labels. You can either remove them outright (e.g. find _STL_CRC_calculate and replace with"STL_CRC_calculate) or use a conditional name mapping using the compiler's __TI_EABI__ predefined symbol. Here's an example of what this looks like in stl_crc_s.asm:
.if __TI_EABI__ .asg STL_CRC_calculate, _STL_CRC_calculate .asg STL_CRC_calculateLowBytes, _STL_CRC_calculateLowBytes .asg STL_CRC_init, _STL_CRC_init .asg STL_CRC_reset, _STL_CRC_reset .endif .global _STL_CRC_calculate .global _STL_CRC_calculateLowBytes .global _STL_CRC_init .global _STL_CRC_reset
#ifdef __TI_EABI__ #pragma RETAIN(STL_HWBIST_restoreContext); #endif #pragma CODE_SECTION(STL_HWBIST_restoreContext, "hwbist"); void STL_HWBIST_restoreContext(void) { ... }
#ifdef __TI_EABI__ #define STL_HWBIST_REF_HANDLE_RESET_FXN __asm(" .ref STL_HWBIST_handleReset") #define STL_HWBIST_LCR_HANDLE_RESET_FXN __asm(" LCR STL_HWBIST_handleReset") #else #define STL_HWBIST_REF_HANDLE_RESET_FXN __asm(" .ref _STL_HWBIST_handleReset") #define STL_HWBIST_LCR_HANDLE_RESET_FXN __asm(" LCR _STL_HWBIST_handleReset") #endif
#ifndef __TI_EABI__ STA_User_spObj.startAddress = (uint32_t)_symval(&_stack); STA_User_spObj.endAddress = (uint32_t)_symval(&_STACK_END); #else STA_User_spObj.startAddress = (uint32_t)_symval(&__stack); STA_User_spObj.endAddress = (uint32_t)_symval(&__TI_STACK_END); #endif