Part Number: TMS320F28379S
Hi Champ,
I have some question about F2837x SafeTI diagnostic library example project.
Could you kindly help on my following question?
In sta_tests.c there have below testing:
Qusetion 1:
For the startAddress, endAddress, goldenCRC are fixed for this device?
If the address is fixed , any document to description these address and the goldenCRC?
case STA_BROM_CRC:
{
//
// Set range to calculate CRC for and the golden CRC value.
//
uint32_t startAddress = 0x3F8000;
uint32_t endAddress = 0x3FFFBF;
uint32_t goldenCRC = 0xBA67176C;
Qusetion 2:
For the startAddress, endAddress, goldenCRC is fixed for this device?
If the address is fixed , any document to description these address and the goldenCRC?
When the address range is 0x78000 to 0x7800F? these address are Z1-LINKPOINTER1 to Z1-LINKPOINTER3.
Z1-LINKPOINTER1 to Z1-LINKPOINTER3 value will be changed by customer if they use DCSM function.
case STA_FLASH_CRC:
{
//
// Set range to calculate CRC for and the golden CRC value.
//
uint32_t startAddress = 0x78000;
uint32_t endAddress = 0x78010;
uint32_t goldenCRC = 0xB70C7E38;