This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello TI expert,
I want to trigger a ITRAP, and use the below method in the main loop.
Define a pointer and point to a illegal address, then write and read the value of it.
But I did not enter into any interrupt.
Is something wrong with my method?
volatile uint32_t *TestOverRangePoint = (uint32_t *)0xFFFFFFFF;
volatile uint32_t TestData = 0;
for (;;)
{
*TestOverRangePoint = 0x01;
TestData = *TestOverRangePoint;
}
Another question is that I want to write the handler for ITRAP.
Does TI provide the example that how to record the return address value on the stack in the ITRAP handler?
Hi W Z,
Please refer to the C28 CPU guide- https://www.ti.com/lit/ug/spru430f/spru430f.pdf section 3.6 and 3.5.2
Easiest way would to execute TRAP #19 instruction that corresponds to ITRAP
Thanks.
Thanks for your help. It is really the easiest way to execute TRAP #19
void trigger_trap19() {
asm(" TRAP #19 ");
}
Could you please help check the below question?
Is something wrong with my method?
I want to test that access to an invaild memory, then enter into the illegal interrupt.
volatile uint32_t *TestOverRangePoint = (uint32_t *)0xFFFFFFFF;
volatile uint32_t TestData = 0;
for (;;)
{
*TestOverRangePoint = 0x01;
TestData = *TestOverRangePoint;
}
Hi WZ,
I want to test that access to an invaild memory, then enter into the illegal interrupt.
Can you point to the reference document for the statement above ?
From C28x Guide I only see the below source for ITRAP:
Thanks
WZ,
That's is Illegal value read from program memory during an instruction fetch.
Illegal OPCODE fetch values are 0000, FFFF, or any value that does not match a defined opcode.
Thanks.
I cannot understand, what is illegal value read from program memory. Could you please show an example?
Got your OPCODE define. But When do the normal coding, how can bring in a not defined opcode?
WZ,
In a case where you start executing from memory which has either all 0000 or FFFF unintentionally then you may end up getting ITRAP
Here is a scenario explained in this e2e : https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1313506/tms320f28335-28335-illegal-instruction-execution-problem/4992071#4992071
Thanks