This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28388D: Program Counter when Resetting

Part Number: TMDSCNCD28388D

Tool/software:

I'm uploading code to my TMDSCNCD28388D board. I have the configuration set to CPU1_FLASH and the linker indicates the code begins (BEGIN) at 0x0008 0000. But, whenever I reset the board in the debugger, the program counter jumps to 0x003F D2AE. How can I fix this so that when I restart the device, it goes back to the start of my code at 0x0008 0000? I tried adjusting the RESET part of the linker from 0x003F FFC0 to 0x0008 0000, but that did not seem to have any effect.