Part Number: TMS320F28335
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE-MOTORCONTROL-SDK, C2000WARE
Tool/software:
HI
I am using the PMSM: FOC Sensorless (Delfino F2833x) program from controlSUITE's High Voltage Motor Control and PFC development kit. I'm testing level3。At present, I have encountered a problem, although it also existed before, my pwm frequency is 10khz, which is stable at the beginning, but then there will be jitter and motor have oscillation , but I changed to 8khz to solve the problem. Now I look at the output of PI, but the previous situation will also occur, I don't know where the problem occurred. I have adjusted the parameters of P and I. Although the motor is stable, the output of PI is quite different from the reference. speed1.SPEED does not correspond to speedref, and speed1.Speedrpm does not correspond to the actual speed. Below is the output of PI I observed with an oscilloscope