Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello, I want to use F28388D, there is a case i have to ask for your help.
if i use F28388D to receive data through high speed SPI (use dma mode). If the length of DMA buffer is 8, when the SPI interface receive 8 data, MCU will get a interrupt from SPI interface and then MCU read SPI data, and then SPI DAM can be ready to receive new data. if MCU do not move away these data, the coming data will miss? right? is there a mechanism which use new data to cover old data? i just want the latest data