This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: TMS320F28366 GND use?

Part Number: TMS320F28377S

Tool/software:

Using TMS320F28377S, Analog GND: PIN17/35/36 feet; Digital GND PIN101 feet,
1. Using a multimeter to test this chip, why are PIN17 and PIN35 connected to PIN101, and PIN36 connected to PIN101?
2. Are the PIN17 and PIN35 connected directly to the PIN101 or are there devices in the middle that filter out the high frequency?
3.PIN36 is not connected to PIN101. What is the voltage between the two pins?

for:Using a multimeter to test this chip, why are PIN17 and PIN35 connected to PIN101, and PIN36 connected to PIN101

How should I use the GND about Analog GND: PIN17/35/36 feet; Digital GND PIN101 feet,?