This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
I received this inquiry from a customer, asking for a mode that would provide precise control of both duty cycle and phase shift:
"
I am using F2837xD MCU for my project to generate PWM signals. I plan to get the data from ADC and use it to control the duty cycle of PWM. Also, there are two PWM channels that their phase difference should be controlled precisely. In other words, I need both high-resolution duty cycle control and phase shift control. I was reading “TMS320x280x, 2801x, 2804x High Resolution Pulse Width Modulator (HRPWM)” app note SPRU924F and it says:
Edge Mode: — The MEP can be programmed to provide precise position control on the rising edge (RE), falling edge (FE) or both edges (BE) at the same time. FE and RE are used for power topologies requiring duty cycle control, while BE is used for topologies requiring phase shifting, e.g., phase shifted full bridge.
Control Mode: — The MEP is programmed to be controlled either from the CMPAHR register (duty cycle control) or the TBPHSHR register (phase control). RE or FE control mode should be used with CMPAHR register. BE control mode should be used with TBPHSHR register.
Apparently none of these configure modes for HRPWM can provide precise control for both duty cycle and phase shift. Can you confirm this or correct me by suggesting a configure mode that I can use for both duty cycle control and phase shift control at the same time?"
Can you help with this?
-RT
Hi RT,
This is correct, the MEP which controls the high resolution edge of the HRPWM module cannot be controlled by both duty and phase control. In instances where HR control, you can implement modes to switch control of the MEP between duty and phase. For instance, we have implemented this in our TIDM-2013 design which you can reference.
Alternately, you can keep the HRPWM in duty control mode and calculate the phase shift manually to make use of HR. We don’t have example code that demonstrates this but it is possible
Regards,
Peter
Dear Peter,
Can you share the concept for calculate the phase shift manually?
Best Regards,
Eric Chen
Hi Eric
Peter is referring to you manually calculating and updating your counter compare values to account for both phase shift and duty cycle. At a high level, here is an example where the PWM begins with rising/falling edges on CMPA = 15 and CMPB = 65. "Phase shift" is applied by updating CMPA and CMPB values to CMPA = 10 and CMPB = 60 rather than writing to TBPHS. This calculation is equivalent to using phase shift of TBPHS = 5. Here's a quick diagram in case it helps:
Best Regards,
Allison
Dear Allison,
Ops! I understood what you mean.
Thanks for the diagram, very clearly!
Best Reagrds,
Eric
Hi Eric,
Just responding here to state we are following up via email. We can post again if further information should be provided on the thread.
Best Regards,
Allison
Hi Eric,
Just wanted to check if there was any follow up from the customer regarding this thread per my last email?
Best Regards,
Allison
Dear Allison,
Thanks for checking with me about the status.
According to the discussion per your email, the customer has no questions for this topic.
You may close the thread, Thank you!
Best Regards,
Eric
Hi Eric,
Thanks for the follow up! I will post a few notes from our mail thread here in case this thread is referred to in the future
Feel free to mark this as resolved to help close the thread!
Best Regards,
Allison