Part Number: TMDSCNCD28379D
Tool/software:
The story is I bought a tmdscncd28379d control card roughly a month ago and am now not able to connect to it. I have uploaded a picture of the board and the error I am getting in code composer.
Some back story, when I first pulled it out of the box and plugged it into my base board, everything worked fine, and I was able to run projects in code composer with no issues. I then let it sit for roughly 1 month, came back to it today, and was not able to connect.
One thing I noticed is that LD2 and LD3 are not lighting up anymore, I know when I first fired the board up those two lights were definitely on, I wonder if that has anything to do with my problem (the picture I attached does not include the base board but LD2 and LD3 do not light up when connected to the base board either)
Another thing to note is I ran the Test Connection diagnosis and the test failed. See picture attached.
Curious if anyone has any ideas on what things I could try to fix this issue.
Thanks,
Ian