This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Power Sequencing Clarification

Expert 4545 points

Part Number: TMS320F28377S

Tool/software:

Hi team,

We have a few questions concerning power up of the part following up on the related thread.

In the designs, VDD is 1.2V. VDDOSC/VDDIO/VDD3V3FL are tied to 3.3V.

One of the designs delays the start of the VDD ramp (1.2V) for a millisecond after VDDOSC/VDDIO/VDD3V3FL and has a high ramp rate to start.

Otherwise, VDD and VDDOSC/VDDIO/VDD3V3FL are always powered on/off together.

Please see the images below.

 

In this case:

VDDOSC is powered when VDD is off for a period of 1 ms at power up.

The initial ramp rate of VDD is 26k v/s for the first 10 us before settling at under 2000 v/s.

Does this meet the requirements:  

"VDDOSC and VDD must be powered on and off at the same time. VDDOSC should not be powered on when VDD is off.”

Supply Ramp Rate between 330 and 10^5 V/s.

Thanks for the support,

Luke