This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
When I am trying to debug LAUNCHXL-F280039C, I got the follow error:
IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 20.0.0.3283)
I have checked the XDS110 version and I have the latest version:
<<<< Device 0 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Embed with CMSIS-DAP
Version: 3.0.0.33
Manufacturer: Texas Instruments
Serial Num: CL391078
Mode: Runtime
Configuration: Standard
I don't know what else I can do.
Hello,
Can you try following the steps in this guide (Table 4-1, page 7) for Error -2131?
Best,
Matt
I will assume that this issue is resolved and close the thread, as its been several weeks without a response.