Part Number: TMS320F28027
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Can the TMS320F28027 achieve >18b PWM resolution? The period isn't so important as long as it is > 10 Hz.
I checked the manual but it seems to focus on high frequency PWM applications. I think the PWM counters are 16b so it might require HWPWM, and this is supported by Table 4-2. I see one example in Table 4-1 for using HWPWM at high resolution, but the capabilities of HWPWM at smaller periods are not clear.
Is there some simple example code on a repo, or do I need to download the whole IDE?