Tool/software:
Hello, I would like to ask why there is no return value when I test using the function STL_March_testRAM
How do I know if the test was successful or not?
I have also tried injecting an error using the function STL_March_injectError
and then use the STL_March_checkErrorStatus function to try to read the status of the error.
But it still returns a successful test