This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU110-U: TMS320F28P650DK

Part Number: TMDSEMU110-U

Tool/software:

Hi,

Am I able to connect UART TX and RX from the MCU to the CTI-20 connector along with the standard 5pin JTAG connection on the XDS110 Debug Probe? Or do I have to use the Auxiliary connector to use UART?

If so, how would I configure that?