Part Number: TMS320F28375D
Tool/software:
Hi experts,
Could you please tell me why there is a difference between the two methods below?
Method 1 did not reduce the current consumption, but method 2 reduced it significantly.
1:Set unused GPIO pins to output, disable internal pull-up, and disconnect external resistors
2:Set unused GPIO pins to input, disable internal pull-up, and connect external pull-down resistors
Both are recommended methods by TRM, but there are differences between them.
Also, I could not find an answer as to the reason in the original thread.

Best regards,
O.H