This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280049C: External mode for debugging

Part Number: LAUNCHXL-F280049C

Tool/software:

I can build and deploy any program on the board. It works correctly.

For debugging purpose, I wanted to connect the board with my computer with the external mode. I have this error bellow.

I have try differents things:

  • In configuration parameter/hardware implementation/target hardware resources/external mode => try both COM port (UART and dataport)
  • Different switchs settings tried
    • S6 : 0 & S8 : 0 
    • S3.1 : 1 & S4 : 1 & S8 : 1


__________________________________________________________________________________________

External Mode Open Protocol Connect command failed  Caused by:

  • Could not connect to target application: XCP internal error: timeout expired, in response to XCP CONNECT command