Part Number: TMS320F280039C
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello,
1. We plan to migrate ECSDA library to 280039, the project is based on C2000Ware_5_04_00_00, the library is from C2000Ware_5_00_00_00 due to the 5_04_00_00 do not include ECSDA library.
when the function first call XCALLOC to allocate memory, the return value is always 0.
I think the heap is not enough when first call XCALLOC.
How can I find this reason?

The heape size and building setting is as follow:


The error is as follow when run calloc function:

2. If I want migrate ECSDA library under the configuration with –opt_for_speed=2, --opt_level=off.
How many heap I need?
3.Also, I try to Increase heap to 0x5ffe, error still occur.