Part Number: TMS320F28377D
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
I am using the TI 28377D processor. I developed my own dual-core project based on the example project "dual core led_ex2_sysconfig" in the examples folder. I can run the project in debug mode with multicore without any issues, but I want to flash the project and run it standalone. After clicking the "Load program" option, I load the .out files first for CPU1 and then for CPU2. However, I cannot see the code running on the processors. It seems that after the .out files are loaded, the processors cannot start the main code, meaning they are stuck in the "halt" state. Could you assist with the automatic startup configuration?