Tool/software:
I have imported the "TIDA- 010938" "10-kW, GaN-based single-phase string inverter with battery energy storage system reference design" into Code Composer Studio (CCS) and am trying to load the code onto the TMS320F28P550SJ9 microcontroller. However, I am getting the following warning during the build process:
#10068-D no matching section (2 warnings)
The warning appears in the linker command file (device_cmd.cmd
) at the following lines:
dclfuncs { *(dclfuncs) } LOAD > FLASH_BANK1,
RUN > RAMGS1,
TABLE(BINIT),
ALIGN(8)
FPUmathTables { *(FPUmathTables) } LOAD > FLASH_BANK0,
RUN > RAMGS1,
TABLE(BINIT),
ALIGN(8)
ISSUE 2
Even if I ignore the linker warnings and proceed to flash the code to the MCU, I encounter a debugging issue during the execution of device_init();
.
The debugger halts specifically after executing the following line inside device_init();
GPIO_setAnalogMode(28U, GPIO_ANALOG_DISABLED);
And the following errors:
No source available for "SysCtl_delay() at my_workspace\...\sinv_F28P55x.out:{3} 0xc057{4}"
No source available for "_system_post_cinit() at my_workspace\..\sinv_F28P55x.out:{3} 0x3fffff{4}"
Microcontroller: TMS320F28P550SJ9PZ
Any guidance on resolving these issues would be greatly appreciated.
Thanks