Part Number: F28M35H52C
Tool/software:
I am trying to use ePWM1 - ePWM6 but only ePWM1 - ePWM4 function. Please see the attached code. Can someone explain what I did wrong?
Thanks,
Michael
//This is code for setting up in the C28 Main()
Uint16 Period = 37500;
InitSysCtrl();
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = ePWM1A
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO1 = ePWM1B
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // GPIO2 = ePWM2A
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // GPIO3 = ePWM2B
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // GPIO4 = ePWM3A
GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // GPIO5 = ePWM3B
GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1; // GPIO6 = ePWM4A
GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 1; // GPIO7 = ePWM4B
GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 1; // GPIO8 = ePWM5A
GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 1; // GPIO9 = ePWM5B
GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 1; // GPIO10 = ePWM6A
GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 1; // GPIO11 = ePWM6B
EDIS;
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
InitFlash();
EPwm1Regs.TBCTL.all = 0; // clear all bits in TBCTL
EPwm1Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”;
EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1”
EPwm1Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode
EPwm1Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear
EPwm1Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear
EPwm1Regs.TBPRD = Period; // 2 kHz PWM frequency
EPwm2Regs.TBCTL.all = 0; // clear all bits in TBCTL
EPwm2Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”;
EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1”
EPwm2Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode
EPwm2Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear
EPwm2Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear
EPwm2Regs.TBPRD = Period; // 2 kHz PWM frequency
EPwm3Regs.TBCTL.all = 0; // clear all bits in TBCTL
EPwm3Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”;
EPwm3Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1”
EPwm3Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode
EPwm3Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear
EPwm3Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear
EPwm3Regs.TBPRD = Period; // 2 kHz PWM frequency
EPwm4Regs.TBCTL.all = 0; // clear all bits in TBCTL
EPwm4Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”;
EPwm4Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1”
EPwm4Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode
EPwm4Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear
EPwm4Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear
EPwm4Regs.TBPRD = Period; // 2 kHz PWM frequency
EPwm5Regs.TBCTL.all = 0; // clear all bits in TBCTL
EPwm5Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”;
EPwm5Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1”
EPwm5Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode
EPwm5Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear
EPwm5Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear
EPwm5Regs.TBPRD = Period; // 2 kHz PWM frequency
EPwm6Regs.TBCTL.all = 0; // clear all bits in TBCTL
EPwm6Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”;
EPwm6Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1”
EPwm6Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode
EPwm6Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear
EPwm6Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear
EPwm6Regs.TBPRD = Period; // 2 kHz PWM frequency
//This is the code from the M3 Main()
HWREG(SYSCTL_MWRALLOW) = 0xA5A5A5A5;
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
FlashInit();
IPCMtoCBootControlSystem(CBROM_MTOC_BOOTMODE_BOOT_FROM_FLASH);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigureCoreSelect(GPIO_PORTA_BASE, 0xFF, GPIO_PIN_C_CORE_SELECT);