This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am trying to use ePWM1 - ePWM6 but only ePWM1 - ePWM4 function. Please see the attached code. Can someone explain what I did wrong?
Thanks,
Michael
//This is code for setting up in the C28 Main() Uint16 Period = 37500; InitSysCtrl(); EALLOW; GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = ePWM1A GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1; // GPIO1 = ePWM1B GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1; // GPIO2 = ePWM2A GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // GPIO3 = ePWM2B GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1; // GPIO4 = ePWM3A GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1; // GPIO5 = ePWM3B GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1; // GPIO6 = ePWM4A GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 1; // GPIO7 = ePWM4B GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 1; // GPIO8 = ePWM5A GpioCtrlRegs.GPAMUX1.bit.GPIO9 = 1; // GPIO9 = ePWM5B GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 1; // GPIO10 = ePWM6A GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 1; // GPIO11 = ePWM6B EDIS; memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); InitFlash(); EPwm1Regs.TBCTL.all = 0; // clear all bits in TBCTL EPwm1Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”; EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1” EPwm1Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode EPwm1Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear EPwm1Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear EPwm1Regs.TBPRD = Period; // 2 kHz PWM frequency EPwm2Regs.TBCTL.all = 0; // clear all bits in TBCTL EPwm2Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”; EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1” EPwm2Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode EPwm2Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear EPwm2Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear EPwm2Regs.TBPRD = Period; // 2 kHz PWM frequency EPwm3Regs.TBCTL.all = 0; // clear all bits in TBCTL EPwm3Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”; EPwm3Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1” EPwm3Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode EPwm3Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear EPwm3Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear EPwm3Regs.TBPRD = Period; // 2 kHz PWM frequency EPwm4Regs.TBCTL.all = 0; // clear all bits in TBCTL EPwm4Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”; EPwm4Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1” EPwm4Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode EPwm4Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear EPwm4Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear EPwm4Regs.TBPRD = Period; // 2 kHz PWM frequency EPwm5Regs.TBCTL.all = 0; // clear all bits in TBCTL EPwm5Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”; EPwm5Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1” EPwm5Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode EPwm5Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear EPwm5Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear EPwm5Regs.TBPRD = Period; // 2 kHz PWM frequency EPwm6Regs.TBCTL.all = 0; // clear all bits in TBCTL EPwm6Regs.TBCTL.bit.CLKDIV = 0; // CLKDIV = “div by 1”; EPwm6Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV = “div by 1” EPwm6Regs.TBCTL.bit.CTRMODE = 2; // count mode = up-down mode EPwm6Regs.AQCTLA.all = 0x0006; // ZRO=set; PRD=clear EPwm6Regs.AQCTLB.all = 0x0006; // ZRO=set; PRD=clear EPwm6Regs.TBPRD = Period; // 2 kHz PWM frequency //This is the code from the M3 Main() HWREG(SYSCTL_MWRALLOW) = 0xA5A5A5A5; memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); FlashInit(); IPCMtoCBootControlSystem(CBROM_MTOC_BOOTMODE_BOOT_FROM_FLASH); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); GPIOPinConfigureCoreSelect(GPIO_PORTA_BASE, 0xFF, GPIO_PIN_C_CORE_SELECT);