This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Inputs of eCAP modules

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hi,

I think there is an error in a comment in example named gpio_ex1_setup that I imported od C2000Ware_5_04_00_00 library.

For eCAP1 module, ECCTL0 is set up like this: ECap1Regs.ECCTL0.bit.INPUTSEL = 7; // Select eCAP1 TO INPUT7

According of the Table 24.1 of TRM, I think the comment is wrong and it should be // Select eCAP1 TO INPUT8.

Please confirm that I'm right because I'm a little confused.

And in the example, we have the same error for all eCAPS.

Regards,

Adrien