Tool/software:
I am using DSP F28335 for running my hardware. For my hardware setup i need multiple interrupt each one dedicated to one separate subsystem.
For sensing the inputs i am using ADC interrupt (SOC EPWM_A_EPWM_B) and after sensing the signals i need to make three subsystem that will take some ADC inputs to generate PWM. Each of this subsystem is triggered using one Hardware interrupt from EPWM blocks. But I am not able to access multiple interrupt, it is showing error " only one instance of hardware interrupt is allowed in a model".
How can i have this separate interrupt for each subsystem?
I have attached the trigger pattern and my code structure as well.