Tool/software:
Hello,
The 100-pin package TMS320F28375D chip has built-in ADC-A and ADC-B modules.
Since there are two ADC modules, asynchronous operation is possible by setting different clock frequencies, resolutions, or sample-and-hold times for each ADC module.
However, the ADC specification table in the datasheet marks characteristics as "Not supported" for the 100-pin package.
I'm curious whether this is simply because it has not been tested or if there is another reason behind it.
Thanks and regards,
Sang-il
Sang,
This is not because of testing and we do not support Asynchronous ADC for 100 pin package.
Best,
Masoud