This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28379D: EPWM 4A not showing pulses

Part Number: TMDSCNCD28379D

Tool/software:

EPWM toggle issue

I am writing a program to generate epwm signals from 5 EPWM modules. 

EPWM 1, EPWM2, EPWM3 are having interrupts. the EPWM pins on the daughter card is working as expected for the first 3 EPWM blocks. 

I am having issues with epwm block 4 and 5, where I cannot see pwm pulses on the EPWM 4A and EPWM 5A pins on the daughter card. (EPWM 4 and EPWM 5 do not have interrupts)

I think I am missing some setting here. Please help me identify which setting I am missing. 

I am using the following settings relevant to the EPWM 4 and 5:

DevCfgRegs.SOFTPRES2.bit.EPWM4 = 1; // ePWM1 is reset
DevCfgRegs.SOFTPRES2.bit.EPWM4 = 0; // ePWM1 is released from reset
DevCfgRegs.CPUSEL0.bit.EPWM4=0; // Enable CPU1 to EPWM1
EPwm4Regs.TBCTL.bit.CTRMODE = 0x3; // Disable the timer
EPwm4Regs.TBCTL.all = 0xC533; 
EPwm4Regs.TBCTL.bit.SYNCOSEL = 1;
EPwm4Regs.TBCTL.bit.PRDLD = 0;
EPwm4Regs.TBCTL.bit.FREE_SOFT = 2;
EPwm4Regs.TBCTL.bit.HSPCLKDIV = 0x0;
EPwm4Regs.TBCTL.bit.CLKDIV = 0x0;
EPwm4Regs.TBCTR = 0x0000; // Clear timer counter
EPwm4Regs.TBPRD = 1999; // EPWM CLK at 50 kHz
EPwm4Regs.TBCTL.bit.PHSDIR = 0; // EPWM
EPwm4Regs.TBCTL.bit.PHSEN = 1;
EPwm4Regs.TBPHS.bit.TBPHS = 1200;
// EPwm4Regs.TBPHS.bit.TBPHS = 0x0000; // Set timer phase
EPwm4Regs.ETPS.all = 0x0000; // Configure interrupt at underflow of epwm1
// EPwm4Regs.ETSEL.all = 0x0009; // Enable interrupt at underflow of epwm1
EPwm4Regs.ETSEL.bit.INTSEL = 1;
EPwm4Regs.ETSEL.bit.INTEN = 0;
EPwm4Regs.ETSEL.bit.INTSELCMP = 0;
// EPwm4Regs.ETSEL.all = 0x0009;
//test 25/11 EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
//test 25/11 EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0;
EPwm4Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
EPwm4Regs.CMPCTL.bit.SHDWBMODE = 0;
EPwm4Regs.CMPCTL.bit.LOADAMODE = 0;
EPwm4Regs.CMPCTL.bit.LOADBMODE = 0;
EPwm4Regs.AQCTLA.bit.CAU = 2; // EPWM1A set to low on TBCTR=CMPA on up count
EPwm4Regs.AQCTLA.bit.CAD = 2; // EPWM1A set to High on TBCTR=CMPA on down count
EPwm4Regs.AQCTLB.bit.CBD = 2;
EPwm4Regs.AQCTLB.bit.CBU = 2;
EPwm4Regs.AQCTLA.bit.PRD = 2;
EPwm4Regs.AQCTLA.bit.ZRO = 2;
EPwm4Regs.DBCTL.bit.OUT_MODE = 0; // Deadband disabled, DB will be generated by the gate drivers
EPwm4Regs.TBCTL.bit.CTRMODE = 0x0; // Enable the timer in count up/down mode

//EPWM 5 Block

DevCfgRegs.SOFTPRES2.bit.EPWM5 = 1; // ePWM1 is reset
DevCfgRegs.SOFTPRES2.bit.EPWM5 = 0; // ePWM1 is released from reset
DevCfgRegs.CPUSEL0.bit.EPWM5=0; // Enable CPU1 to EPWM1
EPwm5Regs.TBCTL.bit.CTRMODE = 0x3; // Disable the timer
EPwm5Regs.TBCTL.all = 0xC533; 
EPwm5Regs.TBCTL.bit.SYNCOSEL = 1;
EPwm5Regs.TBCTL.bit.PRDLD = 0;
EPwm5Regs.TBCTL.bit.FREE_SOFT = 2;
EPwm5Regs.TBCTL.bit.HSPCLKDIV = 0x0;
EPwm5Regs.TBCTL.bit.CLKDIV = 0x0;
EPwm5Regs.TBCTR = 0x0000; // Clear timer counter
EPwm5Regs.TBPRD = 1999; // EPWM CLK at 50 kHz
// EPwm5Regs.TBCTL.bit.PHSDIR = 0; // EPWM
EPwm5Regs.TBCTL.bit.PHSEN = 1;
EPwm5Regs.TBPHS.bit.TBPHS = 1600;
// EPwm5Regs.TBPHS.bit.TBPHS = 0x0000; // Set timer phase
EPwm5Regs.ETPS.all = 0x0000; // Configure interrupt at underflow of epwm1
// EPwm5Regs.ETSEL.all = 0x0009; // Enable interrupt at underflow of epwm1
EPwm5Regs.ETSEL.bit.INTSEL = 1;
EPwm5Regs.ETSEL.bit.INTEN = 0;
EPwm5Regs.ETSEL.bit.INTSELCMP = 0;
// EPwm4Regs.ETSEL.all = 0x0009;
//test 25/11 EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
//test 25/11 EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0;
EPwm5Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
EPwm5Regs.CMPCTL.bit.SHDWBMODE = 0;
EPwm5Regs.CMPCTL.bit.LOADAMODE = 0;
EPwm5Regs.CMPCTL.bit.LOADBMODE = 0;
EPwm5Regs.AQCTLA.bit.CAU = 2; // EPWM1A set to low on TBCTR=CMPA on up count
EPwm5Regs.AQCTLA.bit.CAD = 2; // EPWM1A set to High on TBCTR=CMPA on down count
EPwm5Regs.AQCTLB.bit.CBD = 2;
EPwm5Regs.AQCTLB.bit.CBU = 2;
EPwm5Regs.AQCTLA.bit.PRD = 2;
EPwm5Regs.AQCTLA.bit.ZRO = 2;
EPwm5Regs.DBCTL.bit.OUT_MODE = 0; // Deadband disabled, DB will be generated by the gate drivers
EPwm5Regs.TBCTL.bit.CTRMODE = 0x0; // Enable the timer in count up/down mode

GpioCtrlRegs.GPAGMUX1.bit.GPIO6 = 0;
GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1;

GpioCtrlRegs.GPADIR.bit.GPIO6 = 1;
GpioCtrlRegs.GPAPUD.bit.GPIO6 = 1;

GpioCtrlRegs.GPAGMUX1.bit.GPIO8 = 0;
GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 1;
GpioCtrlRegs.GPADIR.bit.GPIO8 = 1;

GpioCtrlRegs.GPAPUD.bit.GPIO8 = 1;

I am attaching the project. 

Many Thanks in Advance

RCH

  • Hello,

    I will take a look and reply in a timely manner.

  • Hello Stevan.

    I just checked that the EPWM interrupts for blocks 1,2 and 3 are disabled. That is fine. However, EPWM4 and EPWM5 are not showing any pulses on the respective pins on the daughter card. 

    Thanks for your quick response. Please help me with a solution. 

    Regards

    RCH

  • Hello,

    Have you done anything different while configuring EPW3 and EPWM4 for instance?

  • Hi Stevan

    Here is the epwm settings:

    void init_pwm(void)
    {
    EALLOW;


    // Ref to page 108
    ClkCfgRegs.CLKSRCCTL1.bit.OSCCLKSRCSEL = 0x0; // such that oscclk takes from intosc2. intosc2 is 10MHz

    ClkCfgRegs.SYSPLLMULT.bit.IMULT=0x28; // Pll CALCULATED FROM FORMULA IN PAGE 115 (SYS CONTROL)
    ClkCfgRegs.SYSPLLMULT.bit.FMULT=0x00; // Pllsysclk is now at 400MHZ

    ClkCfgRegs.SYSPLLCTL1.bit.PLLEN = 1; // to enable pll
    ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV=0x1; // TO RUN SYSCLOCK IN 200MHz. WHICH IS PLLSYSCLK
    ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV = 4; // Set initial divider at /8
    ClkCfgRegs.SYSPLLCTL1.bit.PLLCLKEN = 1; // Switch over to use PLL output, 200 MHz /8 = 25 MHz
    DelayUs(20/8);

    ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV = 2; // Change to /4 divider
    DelayUs(20/4); // Wait 20 us (just an example)

    ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV = 1; // Change to /2 divider hence fpllclk = 200
    DelayUs(20/4);

    CpuSysRegs.PCLKCR2.bit.EPWM1=1; // TO ENABLE EPWM MODULE 1
    CpuSysRegs.PCLKCR2.bit.EPWM2=1; // TO ENABLE EPWM MODULE 2
    CpuSysRegs.PCLKCR2.bit.EPWM3=1; // TO ENABLE EPWM MODULE 2
    CpuSysRegs.PCLKCR2.bit.EPWM4=1; // TO ENABLE EPWM MODULE 2
    CpuSysRegs.PCLKCR2.bit.EPWM5=1;

    ClkCfgRegs.SYSPLLCTL1.bit.PLLCLKEN = 1; // Switch over to use PLL output

    // SYS CLOCK running at 200 MHz
    ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV = 1; // now EPWMclk is at 100 MHZ

    // EPWM 1block
    DevCfgRegs.SOFTPRES2.bit.EPWM1 = 1; // ePWM1 is reset
    DevCfgRegs.SOFTPRES2.bit.EPWM1 = 0; // ePWM1 is released from reset
    DevCfgRegs.CPUSEL0.bit.EPWM1=0; // Enable CPU1 to EPWM1
    EPwm1Regs.TBCTL.bit.CTRMODE = 0x3; // Disable the timer
    EPwm1Regs.TBCTL.all = 0xC533; // C533 means epwm is at 2khz. c4b3 means epwm is 4khz
    EPwm1Regs.TBCTL.bit.SYNCOSEL = 1;
    EPwm1Regs.TBCTL.bit.PRDLD = 0;
    EPwm1Regs.TBCTL.bit.FREE_SOFT = 2;
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0x0;
    EPwm1Regs.TBCTL.bit.CLKDIV = 0x0; // This means TBCLK=EPWMCLK=100MHz
    EPwm1Regs.TBCTR = 0x0000; // Clear timer counter
    EPwm1Regs.TBPRD = 1999; // EPWM CLK at 50 kHz
    EPwm1Regs.TBPHS.bit.TBPHS = 0x0000; // Set timer phase
    EPwm1Regs.ETPS.all = 0x0000; // Configure interrupt at underflow of epwm1
    EPwm1Regs.ETSEL.all = 0x0009; // Enable interrupt at underflow of epwm1
    EPwm1Regs.ETSEL.bit.INTSEL = 1;
    EPwm1Regs.ETSEL.bit.INTEN = 0;
    EPwm1Regs.ETSEL.bit.INTSELCMP = 0;
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm1Regs.CMPCTL.bit.LOADAMODE = 0;
    EPwm1Regs.CMPCTL.bit.LOADBMODE = 0;
    EPwm1Regs.AQCTLA.bit.CAU = 1; // EPWM1A set to low on TBCTR=CMPA on up count
    // EPwm1Regs.AQCTLA.bit.CAD = 0; // EPWM1A set to High on TBCTR=CMPA on down count
    // EPwm1Regs.AQCTLB.bit.CBD = 0;
    EPwm1Regs.AQCTLB.bit.CBU = 1;
    EPwm1Regs.AQCTLA.bit.PRD = 2;
    EPwm1Regs.DBCTL.bit.OUT_MODE = 0; // Deadband disabled, DB will be generated by the gate drivers
    EPwm1Regs.TBCTL.bit.CTRMODE = 0x0; // Enable the timer in count up/down mode

    //EPWM 2 block
    DevCfgRegs.SOFTPRES2.bit.EPWM2 = 1; // ePWM1 is reset
    DevCfgRegs.SOFTPRES2.bit.EPWM2 = 0; // ePWM1 is released from reset
    DevCfgRegs.CPUSEL0.bit.EPWM2=0; // Enable CPU1 to EPWM1
    EPwm2Regs.TBCTL.bit.CTRMODE = 0x3; // Disable the timer
    EPwm2Regs.TBCTL.all = 0xC533; // C533 means epwm is at 2khz. c4b3 means epwm is 4khz
    EPwm2Regs.TBCTL.bit.SYNCOSEL = 1;
    EPwm2Regs.TBCTL.bit.PRDLD = 0;
    EPwm2Regs.TBCTL.bit.FREE_SOFT = 2;
    EPwm2Regs.TBCTL.bit.HSPCLKDIV = 0x0;
    EPwm2Regs.TBCTL.bit.CLKDIV = 0x0;
    EPwm2Regs.TBCTR = 0x0000; // Clear timer counter
    EPwm2Regs.TBPRD = 1999; // EPWM CLK at 50 kHz
    EPwm2Regs.TBCTL.bit.PHSDIR = 0; // EPWM
    EPwm2Regs.TBCTL.bit.PHSEN = 1;
    EPwm2Regs.TBPHS.bit.TBPHS = 400;
    // EPwm2Regs.TBPHS.bit.TBPHS = 0x0000; // Set timer phase
    EPwm2Regs.ETPS.all = 0x0000; // Configure interrupt at underflow of epwm1
    // EPwm2Regs.ETSEL.all = 0x0009; // Enable interrupt at underflow of epwm1
    EPwm2Regs.ETSEL.bit.INTSEL = 1;
    EPwm2Regs.ETSEL.bit.INTEN = 0;
    EPwm2Regs.ETSEL.bit.INTSELCMP = 0;
    EPwm2Regs.ETSEL.all = 0x0009;
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm2Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    EPwm2Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm2Regs.CMPCTL.bit.LOADAMODE = 0;
    EPwm2Regs.CMPCTL.bit.LOADBMODE = 0;
    EPwm2Regs.AQCTLA.bit.CAU = 1; // EPWM1A set to low on TBCTR=CMPA on up count
    // EPwm2Regs.AQCTLA.bit.CAD = 2; // EPWM1A set to High on TBCTR=CMPA on down count
    // EPwm2Regs.AQCTLB.bit.CBD = 2;
    EPwm2Regs.AQCTLB.bit.CBU = 1;
    EPwm2Regs.AQCTLA.bit.PRD = 2;
    EPwm2Regs.DBCTL.bit.OUT_MODE = 0; // Deadband disabled, DB will be generated by the gate drivers
    EPwm2Regs.TBCTL.bit.CTRMODE = 0x0; // Enable the timer in count up/down mode

    //EPWM 3 block

    DevCfgRegs.SOFTPRES2.bit.EPWM3 = 1; // ePWM1 is reset
    DevCfgRegs.SOFTPRES2.bit.EPWM3 = 0; // ePWM1 is released from reset
    DevCfgRegs.CPUSEL0.bit.EPWM3=0; // Enable CPU1 to EPWM1
    EPwm3Regs.TBCTL.bit.CTRMODE = 0x3; // Disable the timer
    EPwm3Regs.TBCTL.all = 0xC533; // C533 means epwm is at 2khz. c4b3 means epwm is 4khz
    EPwm3Regs.TBCTL.bit.SYNCOSEL = 1;
    EPwm3Regs.TBCTL.bit.PRDLD = 0;
    EPwm3Regs.TBCTL.bit.FREE_SOFT = 2;
    EPwm3Regs.TBCTL.bit.HSPCLKDIV = 0x0;
    EPwm3Regs.TBCTL.bit.CLKDIV = 0x0;
    EPwm3Regs.TBCTR = 0x0000; // Clear timer counter
    EPwm3Regs.TBPRD = 1999; // EPWM CLK at 50 kHz
    EPwm3Regs.TBCTL.bit.PHSDIR = 0; // EPWM
    EPwm3Regs.TBCTL.bit.PHSEN = 1;
    EPwm3Regs.TBPHS.bit.TBPHS = 800;
    // EPwm3Regs.TBPHS.bit.TBPHS = 0x0000; // Set timer phase
    EPwm3Regs.ETPS.all = 0x0000; // Configure interrupt at underflow of epwm1
    // EPwm3Regs.ETSEL.all = 0x0009; // Enable interrupt at underflow of epwm1
    EPwm3Regs.ETSEL.bit.INTSEL = 1;
    EPwm3Regs.ETSEL.bit.INTEN = 0;
    EPwm3Regs.ETSEL.bit.INTSELCMP = 0;
    // EPwm3Regs.ETSEL.all = 0x0009;
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm3Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    EPwm3Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm3Regs.CMPCTL.bit.LOADAMODE = 0;
    EPwm3Regs.CMPCTL.bit.LOADBMODE = 0;
    EPwm3Regs.AQCTLA.bit.CAU = 1; // EPWM1A set to low on TBCTR=CMPA on up count
    // EPwm2Regs.AQCTLA.bit.CAD = 2; // EPWM1A set to High on TBCTR=CMPA on down count
    // EPwm2Regs.AQCTLB.bit.CBD = 2;
    EPwm3Regs.AQCTLB.bit.CBU = 1;
    EPwm3Regs.AQCTLA.bit.PRD = 2;
    EPwm3Regs.DBCTL.bit.OUT_MODE = 0; // Deadband disabled, DB will be generated by the gate drivers
    EPwm3Regs.TBCTL.bit.CTRMODE = 0x0; // Enable the timer in count up/down mode

    //EPWM 4 block

    // to operate EPWM4A, pull up needs to be disabled

    DevCfgRegs.SOFTPRES2.bit.EPWM4 = 1; // ePWM1 is reset
    DevCfgRegs.SOFTPRES2.bit.EPWM4 = 0; // ePWM1 is released from reset
    DevCfgRegs.CPUSEL0.bit.EPWM4=0; // Enable CPU1 to EPWM1
    EPwm4Regs.TBCTL.bit.CTRMODE = 0x3; // Disable the timer
    EPwm4Regs.TBCTL.all = 0xC533; // C533 means epwm is at 2khz. c4b3 means epwm is 4khz
    EPwm4Regs.TBCTL.bit.SYNCOSEL = 1;
    EPwm4Regs.TBCTL.bit.PRDLD = 0;
    EPwm4Regs.TBCTL.bit.FREE_SOFT = 2;
    EPwm4Regs.TBCTL.bit.HSPCLKDIV = 0x0;
    EPwm4Regs.TBCTL.bit.CLKDIV = 0x0;
    EPwm4Regs.TBCTR = 0x0000; // Clear timer counter
    EPwm4Regs.TBPRD = 1999; // EPWM CLK at 50 kHz
    EPwm4Regs.TBCTL.bit.PHSDIR = 0; // EPWM
    EPwm4Regs.TBCTL.bit.PHSEN = 1;
    EPwm4Regs.TBPHS.bit.TBPHS = 1200;
    // EPwm4Regs.TBPHS.bit.TBPHS = 0x0000; // Set timer phase
    EPwm4Regs.ETPS.all = 0x0000; // Configure interrupt at underflow of epwm1
    // EPwm4Regs.ETSEL.all = 0x0009; // Enable interrupt at underflow of epwm1
    EPwm4Regs.ETSEL.bit.INTSEL = 1;
    EPwm4Regs.ETSEL.bit.INTEN = 0;
    EPwm4Regs.ETSEL.bit.INTSELCMP = 0;
    // EPwm4Regs.ETSEL.all = 0x0009;
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm4Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    EPwm4Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm4Regs.CMPCTL.bit.LOADAMODE = 0;
    EPwm4Regs.CMPCTL.bit.LOADBMODE = 0;
    EPwm4Regs.AQCTLA.bit.CAU = 2; // EPWM1A set to low on TBCTR=CMPA on up count
    EPwm4Regs.AQCTLA.bit.CAD = 2; // EPWM1A set to High on TBCTR=CMPA on down count
    EPwm4Regs.AQCTLB.bit.CBD = 2;
    EPwm4Regs.AQCTLB.bit.CBU = 2;
    EPwm4Regs.AQCTLA.bit.PRD = 2;
    EPwm4Regs.AQCTLA.bit.ZRO = 2;
    EPwm4Regs.DBCTL.bit.OUT_MODE = 0; // Deadband disabled, DB will be generated by the gate drivers
    EPwm4Regs.TBCTL.bit.CTRMODE = 0x0; // Enable the timer in count up/down mode

    //EPWM 5 Block
    // to operate EPWM4A, pull up needs to be disabled
    DevCfgRegs.SOFTPRES2.bit.EPWM5 = 1; // ePWM1 is reset
    DevCfgRegs.SOFTPRES2.bit.EPWM5 = 0; // ePWM1 is released from reset
    DevCfgRegs.CPUSEL0.bit.EPWM5=0; // Enable CPU1 to EPWM1
    EPwm5Regs.TBCTL.bit.CTRMODE = 0x3; // Disable the timer
    EPwm5Regs.TBCTL.all = 0xC533; // C533 means epwm is at 2khz. c4b3 means epwm is 4khz
    EPwm5Regs.TBCTL.bit.SYNCOSEL = 1;
    EPwm5Regs.TBCTL.bit.PRDLD = 0;
    EPwm5Regs.TBCTL.bit.FREE_SOFT = 2;
    EPwm5Regs.TBCTL.bit.HSPCLKDIV = 0x0;
    EPwm5Regs.TBCTL.bit.CLKDIV = 0x0;
    EPwm5Regs.TBCTR = 0x0000; // Clear timer counter
    EPwm5Regs.TBPRD = 1999; // EPWM CLK at 50 kHz
    // EPwm5Regs.TBCTL.bit.PHSDIR = 0; // EPWM
    EPwm5Regs.TBCTL.bit.PHSEN = 1;
    EPwm5Regs.TBPHS.bit.TBPHS = 0;
    // EPwm5Regs.TBPHS.bit.TBPHS = 0x0000; // Set timer phase
    EPwm5Regs.ETPS.all = 0x0000; // Configure interrupt at underflow of epwm1
    // EPwm5Regs.ETSEL.all = 0x0009; // Enable interrupt at underflow of epwm1
    EPwm5Regs.ETSEL.bit.INTSEL = 1;
    EPwm5Regs.ETSEL.bit.INTEN = 0;
    EPwm5Regs.ETSEL.bit.INTSELCMP = 0;
    // EPwm4Regs.ETSEL.all = 0x0009;
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    //test 25/11 EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm5Regs.CMPCTL.bit.SHDWAMODE = 0; // shadow A mode disabled
    EPwm5Regs.CMPCTL.bit.SHDWBMODE = 0;
    EPwm5Regs.CMPCTL.bit.LOADAMODE = 0;
    EPwm5Regs.CMPCTL.bit.LOADBMODE = 0;
    EPwm5Regs.AQCTLA.bit.CAU = 2; // EPWM1A set to low on TBCTR=CMPA on up count
    EPwm5Regs.AQCTLA.bit.CAD = 2; // EPWM1A set to High on TBCTR=CMPA on down count
    EPwm5Regs.AQCTLB.bit.CBD = 2;
    EPwm5Regs.AQCTLB.bit.CBU = 2;
    EPwm5Regs.AQCTLA.bit.PRD = 2;
    EPwm5Regs.AQCTLA.bit.ZRO = 2;
    EPwm5Regs.DBCTL.bit.OUT_MODE = 0; // Deadband disabled, DB will be generated by the gate drivers
    EPwm5Regs.TBCTL.bit.CTRMODE = 0x0; // Enable the timer in count up/down mode


    PieVectTable.EPWM1_INT = &phA_0;
    IER |= M_INT3; // means enter third group of Interrupts Page 95
    IER |= M_INT1;
    PieCtrlRegs.PIEIER3.bit.INTx1=1; // interrupt 3.1= epwm 1 INT page 95

    PieVectTable.EPWM2_INT = &phB_0;
    IER |= M_INT3; // means enter third group of Interrupts Page 95
    IER |= M_INT2;
    PieCtrlRegs.PIEIER3.bit.INTx2=1; // interrupt 3.1= epwm 1 INT page 95

    PieVectTable.EPWM3_INT = &phC_0;
    // IER |= M_INT3; // means enter third group of Interrupts Page 95
    // IER |= M_INT3;
    // PieCtrlRegs.PIEIER3.bit.INTx3=1; // interrupt 3.1= epwm 1 INT page 95

    CpuSysRegs.PCLKCR2.bit.EPWM3=1; // TO ENABLE EPWM MODULE 2
    CpuSysRegs.PCLKCR2.bit.EPWM4=1; // TO ENABLE EPWM MODULE 2
    CpuSysRegs.PCLKCR2.bit.EPWM5=1; // TO ENABLE EPWM MODULE 2

    // PieVectTable.TIMER1_INT = &timer1_intsr;

    // Enable global Interrupts and higher priority real-time debug events:
    EINT; // Enable Global interrupt INTM
    ERTM; // Enable Global realtime interrupt DBGM
    asm(" EALLOW"); // Enable EALLOW protected register access
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1; // TBCLK to ePWM modules enabled
    EDIS;


    // Enable CPU INT3 which is connected to EPWM1-3 INT:
    // IER |= M_INT13;


    }

    For GPIOs, I have:

    GpioCtrlRegs.GPAGMUX1.bit.GPIO0 = 0; // 0|0=GPIO 0|1=EPWM1A 0|2=rsvd 0|3=rsvd
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // 1|0=GPIO 1|1=rsvd 1|2=SDAA 1|3=rsvd
    GpioCtrlRegs.GPAGMUX1.bit.GPIO1 = 0; // 0|0=GPIO 0|1=EPWM1B 0|2=rsvd 0|3=MFSRB
    GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 1;
    GpioCtrlRegs.GPADIR.bit.GPIO0 = 1;
    GpioCtrlRegs.GPADIR.bit.GPIO1 = 1;

    GpioCtrlRegs.GPAGMUX1.bit.GPIO2 = 0; // 0|0=GPIO 0|1=EPWM1B 0|2=rsvd 0|3=MFSRB
    GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 1;
    GpioCtrlRegs.GPAGMUX1.bit.GPIO3 = 0; // 0|0=GPIO 0|1=EPWM1B 0|2=rsvd 0|3=MFSRB
    GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1;
    GpioCtrlRegs.GPADIR.bit.GPIO2 = 1;
    GpioCtrlRegs.GPADIR.bit.GPIO3 = 1;


    GpioCtrlRegs.GPAGMUX1.bit.GPIO4 = 0; // 0|0=GPIO 0|1=EPWM1B 0|2=rsvd 0|3=MFSRB
    GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 1;
    GpioCtrlRegs.GPAGMUX1.bit.GPIO5 = 0; // 0|0=GPIO 0|1=EPWM1B 0|2=rsvd 0|3=MFSRB
    GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 1;
    GpioCtrlRegs.GPAGMUX1.bit.GPIO6 = 0; // 0|0=GPIO 0|1=EPWM1B 0|2=rsvd 0|3=MFSRB
    GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1;
    GpioCtrlRegs.GPADIR.bit.GPIO4 = 1;
    GpioCtrlRegs.GPADIR.bit.GPIO5 = 1;
    GpioCtrlRegs.GPADIR.bit.GPIO6 = 1;
    GpioCtrlRegs.GPAPUD.bit.GPIO6 = 0; // Enable pull-up on GPIO6 (EPWM4A)
    GpioCtrlRegs.GPAPUD.bit.GPIO8 = 0; // Enable pull-up on GPIO8 (EPWM5A)

    GpioCtrlRegs.GPAGMUX1.bit.GPIO7 = 0;
    GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 1;
    GpioCtrlRegs.GPADIR.bit.GPIO7 = 1;
    GpioCtrlRegs.GPAGMUX1.bit.GPIO8 = 0;
    GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 1;
    GpioCtrlRegs.GPADIR.bit.GPIO8 = 1;

    Regards

    Rupak

  • Hello,

    Thank you for providing more details. I checked your configuration and there is an issue with the AQCTLA and AQCTLB register set up for EPWM4 and EPWM5.

    EPwm4Regs.AQCTLA.bit.CAD = 2; // EPWM1A set to High on TBCTR=CMPA on down count
    EPwm4Regs.AQCTLB.bit.CBD = 2;
    EPwm4Regs.AQCTLB.bit.CBU = 2;
    EPwm4Regs.AQCTLA.bit.PRD = 2;
    EPwm4Regs.AQCTLA.bit.ZRO = 2;

    You are setting up your ePWM to go high on CAD, CBD events etc. But you are never clearing it and forcing it to go low, so the output would not toggle. It would just stay high. You configured it correctly for other EPWMs.

    EPwm3Regs.AQCTLA.bit.CAU = 1; // EPWM1A set to low on TBCTR=CMPA on up count
    // EPwm2Regs.AQCTLA.bit.CAD = 2; // EPWM1A set to High on TBCTR=CMPA on down count
    // EPwm2Regs.AQCTLB.bit.CBD = 2;
    EPwm3Regs.AQCTLB.bit.CBU = 1;
    EPwm3Regs.AQCTLA.bit.PRD = 2;

    Please refer to the register description (AQCTLA and AQCTLB) in device TRM to set up the correct actions: https://www.ti.com/lit/ug/spruhm8k/spruhm8k.pdf

    Best regards,

    Stevan D.