This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: ADC ePWM construction C2000 package matlab simulink

Part Number: TMS320F28379D

Tool/software:

I am using the C2000 support package in the matlab simulink. I want a 20khz and 0.5 duty cycle. Hence, I have set the TBPRD at 2500 and CMP value at 1250. I have attached my Algorithm image from ADC to ePWM. For ADCAIN3 the output ePWM1 and ePWM4 are blue and pink waveform. For ADCBIN2 the output ePWM2 and ePWM3 are green and yellow waveform. The switch and sign block are used to control the half cycle of Vac reference voltage/signal. The PWM signal is generated based on the digital representation of the analog value read from the input. I am using transport delay to shift the signal from positive half cycle to the negative half cycle as shown in the image attached. The transport delay is set to 0.05 of the time delay. ePWM1 CAU: clear CAD: set. ePWM4 CAU: set CAD: clear. ePWM2 CAU: clear CAD: set. ePWM3 CAU: set CAD: clear. The deadband supposed to be set at 900ns. I have tried to used the deadband however, the duty cycle/width of the PWM only changes. My problem is the waveform yellow ePWM4 and blue ePWM3 are overlapping. How to fix this issue? How to produce the signal at negative half cycle of Vac reference voltage/signal.

Thank you.