This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Averaging Oversampled ADC Signal over PWM cycle with Simulink

Part Number: LAUNCHXL-F28379D


Tool/software:

Hi Community,

i try to average a voltage Signal over a PWM cycle (10 kHz Signal). Goal is to trigger the ADC measurment with the ePWM signal and then oversample for example 200 values of the adc signal during the pwm cycle and calculate the average of these values for the next cycle. (See signal image) The AEC ist triggered according to the settings in the image.

Thank you and kind regards

Chris