This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Error While Debugging

Part Number: LAUNCHXL-F28379D

Tool/software:

Hello E2E Experts,

Good day.

Present Device: LAUNCHXL-F28379D
CCS Version : 20.1.0.6_1.7.0
  1. When the device is connected, the CCS studio is unable to detect the board automatically.
    Could you please help us in confirming if the version of CCS supports the device we are using?
    Or, kindly let us know which version of CCS is compatible with the device.
    We noticed the same issue on the other laptop also.
  2. Also, when checked in the port properties, we noticed that there is a problem status:  0xC00000E5 , as shared in the snapshot below.
    Kindly let us know how to resolve these issues.

Regards,

TICSC

  • Hi,

    When the device is connected, the CCS studio is unable to detect the board automatically.
    Could you please help us in confirming if the version of CCS supports the device we are using?
    Or, kindly let us know which version of CCS is compatible with the device.
    We noticed the same issue on the other laptop also.

    This version of CCS should support F2837xD and all other C2000 MCUs. When installing CCS, was 'C2000 MCUs' selected such as in the previous screenshot? 

    If it wasn't or you're not sure, no problem. You can navigate to Help > Check for Updates and update C2000 device support files. Refer to this guide for more information: Update Overview — Code Composer Studio 20.1.0 Documentation

    Also, when checked in the port properties, we noticed that there is a problem status:  0xC00000E5 , as shared in the snapshot below.
    Kindly let us know how to resolve these issues.

    There seems to potentially be an issue with the device driver. Let's trying to update it by following these steps. The paths are referring to an older CCS, but the steps remain the same: XDS110 Debug Probe

    (+) LAUNCHXL-F280025C: CCS Updating firmware bricks board

    Best Regards,

    Aishwarya