Tool/software:
If this feature has not be included, I suggest that it can be featured in further updates of CCS Theia.
Thanks a lot.
It's the CCS Theia 1.5.1.000011, instead of the Eclipse-based version.
Please note that CCS 20 is based on Theia. The last Eclipse version is CCS 12.8.1.
Every version of CCS after that version is based on Theia:
In CCS 20.1.1, the watch view looks like: