This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: The reason why motor parameter measurement and extraction values cause an error

Part Number: TMS320F28P650DK

Tool/software:

Hello.
I'm writing because I have a question.
The TI resistance parameter extraction causes an error with the motor meter when extracting the resistance value.
The motor resistance meter measures 71mHm, but when measured with the TI motor parameter meter
44 mHm is measured, the error rate of the motor resistance meter is shown to be 0.02%.

1. The reason for the error.
2. Error tolerance
3. a way to reduce the error rate

Please reply.