This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-HV-1PH-DCAC: Reference design enquiry for our requirements with 48Vdc input

Part Number: TIDM-HV-1PH-DCAC
Other Parts Discussed in Thread: PMP23069

Tool/software:

Hi sir,

I reviewed TIDM-HV-1PH-DCAC document and we want to design 5KVA single phase inverter  with 48Vdc input and we require pure sign wave output. Does this reference will  support our requirements.

Please help us.

Thanking you...

  • Hello Ranjith

    This design is rated for 600VA and 380V DC input voltage. Hence it is much different in terms of specifications. So you cannot follow the hardware design as it is. You can adopt the control algorithm and device configuration from this design.

    If you are going to run your inverter in grid connected mode (not in standalone mode), then you can follow pmp23069. This is PFC that can run in grid-connected inverter mode. Its rating is 3.3 kW.

    Thank you

    Amir Hussain 

  • Thank you for your valuable input,

    Can you please suggest any other design which meets our specification that, input 48Vdc(nominal) and 230Vac output with 5KVA load for home inverter online UPS design. And the output should be pure sine wave.

    Thank you...

  • Hello Ranjit

    Unfortunately, we do not have a ref design that matches the above specification.

    Thank you

    Amir Hussain